KAS Simulator Axes Tab

Axes Tab

Figure 6-70: Axes Tab

The dashed line (or dotted line) represents the Reference Position in User units.
When the is solid line (or normal line) visible, it represents the Actual Position in User units.

Below the disk, the reference position for the associated axis is represented in the following format:

Range value (Modulo value according to the periodicity)

As shown on the figure below, the Error command (in the contextual menu of the axis tab) is used to simulate an error on an axis (then you can see the impact on the HMIClosed"Human-machine interfaces " Also known as computer-human interfaces (CHI), and formerly known as man-machine interfaces, they are usually employed to communicate with PLCs and other computers, such as entering and monitoring temperatures or pressures for further automated control or emergency response and implement counter-measures if necessary).

Set Axis in Error Mode

Figure 6-71: Set Axis in Error Mode

The drive becomes Red when it is set to Error . Motion State Machine

To deselect an axis already selected (blue rectangle), click on the white surrounded outside border of the axis tab.

Deselect an Axis

Figure 6-72: Deselect an Axis

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen